Skip to main content
Macdog
Associate III
March 21, 2023
Solved

How to install for windows 10?

  • March 21, 2023
  • 1 reply
  • 2230 views

I have (I believe) installed all the prerequisites and added the paths to STM32CubeMX and STMCUFinder. However I cannot use the extension as the commands are not available.

0693W00000aJMiCQAW.jpgIf I try to run the command via the command palette, I get a "command not found" error popup.

0693W00000aJMibQAG.jpgThanks in advance for any ideas or help to move forward.

This topic has been closed for replies.
Best answer by Macdog

Well, turns out I was using an older version of VSCode from November 2022 (1.74.x). Updating to the February 2023 (1.76) version the STM32 PROJECT MANAGER and RESOURCES items are visible in the LH pane. Now to see if it works.

1 reply

Macdog
MacdogAuthorBest answer
Associate III
March 21, 2023

Well, turns out I was using an older version of VSCode from November 2022 (1.74.x). Updating to the February 2023 (1.76) version the STM32 PROJECT MANAGER and RESOURCES items are visible in the LH pane. Now to see if it works.