Skip to main content
Associate
October 13, 2025
Question

STM32CubeIDE for VSCode 3.6.4 STM32N6 Support

  • October 13, 2025
  • 3 replies
  • 408 views

Hello,

 

When I attempt to set up an existing project or create a new project with the VSCode plugin version 3.6.4, I do not see the STM32N6 family as an available/supported device. Am I missing a package or is something corrupted in my installation?

aroby95_0-1760368513110.png

 

3 replies

Cartu38 OpenDev
Graduate II
October 13, 2025

@aroby95 
Works for me

Cartu38OpenDev_0-1760369169012.png

Based on VSCode integrated terminal, what is output of following command ?

cube pack sync

Cartu38OpenDev_1-1760369285720.png

If any fail reason why I guess ... (are you connected to internet, any firewall or ?)

ST Employee
October 14, 2025

Thanks, @Cartu38 OpenDev, for sharing this very valuable comment.

@aroby95, please give it a try, and if you encounter any issues, possibly you are facing: https://community.st.com/t5/stm32cubeide-for-visual-studio/cube-pack-sync-error-via-vscode-proxy/td-p/847146 

Could you confirm ?

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
Julien D
ST Employee
October 17, 2025

@aroby95, did you solved your issue by some way?

If not, as suggested, could you execute the cube pack sync command in VSCode integrated terminal and paste here the result?

JulienD_0-1760681321675.png

 

 

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.