Solved
VS-Code extension 3.5.1: HardFault during USBX initialization on STM32U5A5
- July 28, 2025
- 3 replies
- 698 views
I'm trying the new VS-Code extension 3.5.1, but I end up in the HardFault_Handler function during the initialization, in the "MX_USBX_Device_Init" function. The same project works correctly when using the "cortex-debug" plugin (separate VS Code profile to avoid conflicts).
It's a very simple project where I did the very minimal config to enable USBX, and "UX Device HS -> Device Class HS -> HID -> MSC" on my STM32U5A5AJH6Q. The IOC file is attached.
It crash in the function "USBD_FrameWork_MSCDesc", at line
/* Append Endpoint descriptor to Configuration descriptor */
__USBD_FRAMEWORK_SET_EP((pdev->tclasslist[pdev->classId].Eps[1].add),
(USBD_EP_TYPE_BULK),
(uint16_t)(pdev->tclasslist[pdev->classId].Eps[1].size),
(0U), (0U));