ADC Injected Conversion
I am trying to use the Pin ADC1_EXT11(PC11) and ADC1_EXT15(PA15) as ADC input sampling pins. But in the setting given in Cube IDE, if i enable injected conversion, additionally 2 pins are automatically getting configured for some reason. I don't know why? Is it that the, pins PA15 and PC11 are interrupt pins and whenever interrupt is triggered in those pins, ADC samples from pins PA6 and PB0.?

and what is the difference in the below highlighted options