After upgrading CubeMx plugin from 6.10.0 to 6.11.0, MCU temperature sensor is no longer supported
I'm using STM32CubeIDE and targeting STM32H745IIK6. When I was using the CubeMx plugin version 6.10.0, I was able to enable the temperature sensor input on ADC3:

After upgrading to CubeMx 6.11.0 with FW package H7_v1110.zip, this option (as well as the two inputs listed immediately before and immediately after it) are now gone:


With upgraded SW/FW:

The three options that used to be listed towards the end of the page, between the "IN16" input and the "EXTI Conversion Trigger" are missing. Are they available elsewhere now?