Skip to main content
LJIAN.11
Visitor II
July 1, 2022
Question

As shown in the following figure, there are multiple page ghosting in cubemx when setting project properties. How can I solve it?

  • July 1, 2022
  • 7 replies
  • 2709 views

0693W00000QKGUkQAP.png

This topic has been closed for replies.

7 replies

ST Employee
July 8, 2022

Hello @LJIAN.1​ ,

Thanks for your feedback,

Could you please specify the CubeMX version and which OS are you using ?

Sara.

AlgoOy
Associate
August 17, 2022

I have the same problem, and I use the latest CubeMX​. I run this software in windows10.

Tesla DeLorean
Guru
August 17, 2022
Tips, Buy me a coffee, or three.. PayPal VenmoUp vote any posts that you find helpful, it shows what's working..
AlgoOy
Associate
August 17, 2022

thank you.

Aymen CHAKROUN
ST Employee
August 17, 2022

Hi @LJIAN.1​  and @AlgoOy​ ,

Can you give us the Wind10 PC HW config:

  • RAM ?
  • CPU name and Freq ?
  • PC Model ?

Can you also monitor your available PC RAM availability when you observe this issue, I guess RAM availability issue.

Can you confirm that this behavior is systematic even with a PC reboot ?

Regards,

Aymen.

AlgoOy
Associate
August 17, 2022

​CPU:

AMD Ryzen 7 5800H with Radeon Graphics 

​Base speed: 3.20 GHz

GPU:

NVIDIA GeForce RTX 3070 Laptop GPU

Driver version: 31.0.15.1694

​Memory:

32.0 GB

Speed: 3200 MHz

Available 16.4 GB

In use (Compressed) 11.4 GB (467 MB)

PC Model:

Legion R9000P2021H

Processor AMD Ryzen 7 5800H with Radeon Graphics      3.20 GHz

Installed RAM 32.0 GB (27.9 GB usable)

This kind of situation happened every time, and even if I restart the computer.

殷亚鑫.1
Visitor II
September 12, 2022

I have the same problem too !!

BCHEN.2
Visitor II
September 14, 2022

I have the same problem too !!

BCHEN.2
Visitor II
October 25, 2022

I have the same problem too !!

LYao.2
Visitor II
February 18, 2023

I have the same problem too !!