Break at address 0x18003A1A with no debug information in CubeMX-generated project

I generated a project using STM32CubeMX for the STM32N6570-DK board.
Steps performed:
Generated code using CubeMX (default configuration)
Imported project into STM32CubeIDE
Built the project successfully (no build errors)
Attempted to run/debug the application
During programming / start of execution, the debugger stops with the following message:
Break at address “0x18003A1A” with no debug information available, or outside of program code