Can't install STMCUFinder on MacOS Ventura 13.3.
This is a prerequisite for the VSCode extension which is why I am asking here.
Steps to reproduce:
Download the setup file
Per Readme.html, open a terminal, navigate to the en folder and run the following command: sudo xattr -cr ./SetupSTMCUFinder-5.0.0.app
Enter password
Exit the terminal
Open Finder
in the en folder, double click on SetupStMCUFinder-5.0.0
Setup always complains that "java" cannot be opened because the developer cannot be verified
Show package contents of SetupStMCUFinder-5.0.0
Right click on SetupTMCUFInder-5_0_0 and select Open
Setup always complains that "java" cannot be opened because the developer cannot be verified
I need to get VSCode running but until I can get this prerequisite running, I don't believe it will have full functionality.
Thank you in advance for your assistance!
Clark