clarity on external loader using stm32h750xbhx
by using the stm32h750xbhx i created two projects. one is bootloader and other is application. we are trying to use external flash to store the application, as the file size is much larger than the capacity of the internal flash.
and we are trying to flash the bootloader to internal flash and from the bootloader we will jump to the application program which is in external flash.(can we do that directly or we need qspi to do the jump also).
and we are planning to run the application on the external flash like xip(execute in place).
what is the best way to flash the application to the external flash.
can we do the whole process like this and what is the best procedure to follow
if possible clarify the confusion around the qspi intialization, where to do and when to do.