Code generation issue with Discovery board B-L072Z-LRWAN1
I have a Discovery board B-L072Z-LRWAN1 and I am trying to set up a project using CubeIDE but get the following,

So I check to see if the L0 & LRWAN packages are in the repository,

Yes, they're there. I click OK & Cube carries on setting itself up & up pops the ioc window. I press configure & generate & get some C code but the build option is greyed out.
What am I missing here?