Skip to main content
MSilv.5
Visitor II
February 26, 2023
Question

Crash when launch stm32 new project or when update embedded ...

  • February 26, 2023
  • 1 reply
  • 1133 views

Hi,

I installed the latest version of STM32IDE on Mac (Ventura 13.2.1 (22D68))

STM32CubeIDE

Version: 1.11.2

Build: 14494_20230119_0724 (UTC).

the interface opens without problems. When instead I try to create a new project, a satellite update program opens and everything closes (crash), I can't get out of it.

Can you help me ? Thank you

This topic has been closed for replies.

1 reply

Julien D
ST Employee
February 27, 2023

Hello,

I add STM32CubeMX tag since these updates are initiated by MX, not STM32CubeIDE directly.

To ease the analysis could you share the related Crash Report if any ? Launch the Console application and navigate to Crash Reports from the left panel.

In the meantime you can try to put the MX firmware update in offline mode, and confirm if this workarounds the crash. The option can be found in Preferences > STM32Cube > Firmware Updater (a restart of STM32CubeIDE might be then required).

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.