Skip to main content
Marco1
Associate III
January 25, 2023
Solved

Cube Bug on MCU SELECTOR ?

  • January 25, 2023
  • 2 replies
  • 935 views

Hi,

i need to find a mcu with 2 usb, min 512k of total ram and min 1024k of flash.

When i put RAM and flash on selector, the result is mcu without USB, but you can see on list many mcu with 2 USB.

The result is worst if you put on selector directly 2 usb ( without flash and ram )... the mcu showed are different.

Its a selector bug ?

Sorry for my english !

Regards

0693W00000Y99yJQAR.png 

This topic has been closed for replies.
Best answer by Ghofrane GSOURI

Hello @Marco​ 

First let me thank you for posting.

I confirm the issue on my side, it has been reported to STM32CubeMX development team .

Internal ticket number:  143798(This is an internal tracking number and is not accessible or usable by customers).

I will keep you posted with updates.

Thx

Ghofrane

2 replies

Ghofrane GSOURI
Ghofrane GSOURIBest answer
Technical Moderator
January 26, 2023

Hello @Marco​ 

First let me thank you for posting.

I confirm the issue on my side, it has been reported to STM32CubeMX development team .

Internal ticket number:  143798(This is an internal tracking number and is not accessible or usable by customers).

I will keep you posted with updates.

Thx

Ghofrane

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
Piranha
Principal III
January 27, 2023

The MCU data is wrong for many parts. And the filter functionality itself is also full of issues. For example, there are two places where one can set the Ethernet feature and those return different results:

Communication Interface => Ethernet Port [>=1]: 585 devices.

Other Interface => Additional Interface => Ethernet [1]: 603 devices.