Associate II
April 15, 2024
Solved
CubeIDe 1.15.0 FW_f4_1.28.0 USB CDC not working
- April 15, 2024
- 1 reply
- 1992 views
Hello, I have a very simple code written with earlier versions of CubeIDE and FW_F4_1.26.2 for STM32F405rgt6
It is a very simple code, just sending a message via USB as a CDC Device . If I download the old .elf file to controller, everything works fine, but windows won't see the device nor get the messages when I compile it with 1.28.0 FW .
Is there a difference with usage? Or is there a bug with this?
Here is the code.