Skip to main content
debugging
Lead
September 19, 2024
Question

CubeMX 6.12.0 & 6.12.1 MainProjectManager:1100 - Error after a good Download of DB/Firmware Package / Unzip File : DB.6.0.111.tar.bz2

  • September 19, 2024
  • 4 replies
  • 1207 views

Ubuntu 23.10

Tried to load an older project in 6.12.0, CubeMx Asked to convert or continue. Selecting continue.

IT start to unzip the tarball and then stops. cube has no error screen, but the log shows as follows

Updating to CubeMX 6.12.1 yields  the  same result. Looked up the tabrall and it can be opened.

Note: With the option MIGRATE could open the project.

2024-09-19 20:55:38,081 [INFO] I2cTimingTraitement:330 - 0x10C0ECFF
2024-09-19 20:55:38,101 [INFO] I2cTimingTraitement:330 - 0x108082C4
2024-09-19 20:55:39,806 [INFO] MicroXplorer:468 - Change Database Path :
2024-09-19 20:55:39,806 [INFO] MicroXplorer:498 - Change Database Version : DB.6.0.120
2024-09-19 20:55:39,900 [WARN] ThirdParty:871 - waiting for thirdparty lock release [close project]
2024-09-19 20:55:39,900 [INFO] ThirdParty:873 - entering critical section [close project]
2024-09-19 20:55:39,900 [INFO] ThirdParty:883 - exiting critical section [close project]
2024-09-19 20:55:39,911 [INFO] PinOutPanel:1561 - setPackage(No Configuration,No Configuration)
2024-09-19 20:55:57,359 [INFO] MicroXplorer:468 - Change Database Path :
2024-09-19 20:55:57,359 [INFO] MicroXplorer:498 - Change Database Version : DB.6.0.120
2024-09-19 20:55:57,472 [WARN] ThirdParty:871 - waiting for thirdparty lock release [close project]
2024-09-19 20:55:57,472 [INFO] ThirdParty:873 - entering critical section [close project]
2024-09-19 20:55:57,472 [INFO] ThirdParty:883 - exiting critical section [close project]
2024-09-19 20:55:57,482 [INFO] PinOutPanel:1561 - setPackage(No Configuration,No Configuration)
2024-09-19 20:55:57,509 [INFO] UtilMem:75 - Begin LoadConfig() Used Memory: 718350328 Bytes (1077936128)
2024-09-19 20:55:59,023 [INFO] FileExtend:240 - Unzip File : DB.6.0.111.tar.bz2
2024-09-19 20:55:59,024 [INFO] FileExtend:305 - Tar/BZip2 Deflate
2024-09-19 20:57:03,937 [INFO] LoadServerPackagesThread:196 - End of LoadServerPackages Thread
2024-09-19 20:57:04,074 [INFO] CheckServerUpdateThread:120 - End of CheckServer Thread
2024-09-19 20:57:04,079 [ERROR] MainProjectManager:1100 - Error after a good Download of DB/Firmware Package

4 replies

Technical Moderator
September 19, 2024

Hello @debugging 

Ubuntu 23.10 is not officially supported by STM32CubeMX. Below is the list of OS supported (in RN):

SouhaibMAZHOUD_0-1726753469266.png

 

 

Thank you,

Souhaib

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
debugging
debuggingAuthor
Lead
September 21, 2024

Thank you, but I very much doubt this has to do with Ubuntu. What points to that this is Ubuntu related ? anyone tried with an older Ubuntu version to NOT convert a project ?

Even 23.10 is already not supported by Canonical and dev system often need use latest releases of OSes for example for my particular device I need to interact with the device using the latest Linux kernel. Can't wait for ST to catch up.

Visitor II
May 23, 2025

I have the same problem under windows 10.

 

STM32cubefirm.pngSTM32Cubefrim_.jpg

The downloadprocess take some minutes and quit without any improvement.

debugging
debuggingAuthor
Lead
June 9, 2025

Sorry, I am using Ubuntu 24.10 now and MX works fine.  I think I recall it has to do with an issue in Eclipse, but can;d find it anymore. Perhaps you can try another java version. Here is mine

$update-java-alternatives --list
java-1.11.0-openjdk-amd64 1111 /usr/lib/jvm/java-1.11.0-openjdk-amd64
java-1.21.0-openjdk-amd64 2111 /usr/lib/jvm/java-1.21.0-openjdk-amd64
java-1.8.0-openjdk-amd64 1081 /usr/lib/jvm/java-1.8.0-openjdk-amd64

 https://learnubuntu.com/change-java-version/