CubeMX code generation fails with specific X-CUBE-AI settings
Hello,
I'm having trouble getting the CubeMX code generation to work reliably with X-CUBE-AI package.
After first adding X-CUBE-AI to the project, and adding one of the models from the ST model zoo, i get this warning:

If i click Yes, the code generation takes about 5 minutes and works.
Note that in the above picture, X-CUBE-AI ExtMemLoader is selected. This is also where the warning comes from. AFAIK, i don't need X-CUBE-AI ExtMemLoader, just the Application. If i remove the checks from the checkboxes "Artificial Inteligence X-Cube-Ai" and "Device Appliccation", and then reopen MX, the X-CUBE-AI ExtMemLoader will disappear, and just the X-CUBE-AI Application remains. However, after trying to generate code with that setup, the code generation hangs to the below phase of code generation:

At that state, the OpenJDK Platform binary uses over 6000 MB of RAM, and about 10% of my CPU but seemingly nothing happens. I waited over the weekend to see if the generation would finish but it did not, then I retried multiple times, waiting about 20 minutes each time and it always hangs there.
Also there are some paths in the mx-generated.cmake which are wrong i think, as the code fails to build:
[0/1] Re-running CMake...Build type: Debug
-- Configuring done (0.4s)
CMake Error at mx-generated.cmake:147 (target_sources):
Cannot find source file:
C:/Users/tuoma/STM32Cube/helium_test/Src/audio_network.c
Call Stack (most recent call first):
CMakeLists.txt:40 (include)
CMake Error at mx-generated.cmake:137 (target_sources):
Cannot find source file:
C:/Users/tuoma/STM32Cube/helium_test/Middlewares/ST/AI/Npu/ll_aton/ecloader.c
Call Stack (most recent call first):
CMakeLists.txt:40 (include)
CMake Error at mx-generated.cmake:136 (add_library):
No SOURCES given to target: ST
Call Stack (most recent call first):
CMakeLists.txt:40 (include)
CMake Generate step failed. Build files cannot be regenerated correctly.
but builds after adjusting the paths:

and fixing missing include in generated app_x-cube-ai.c file
C:/Users/tuoma/STM32Cube/helium_test/CORTEX_HELIUM/Appli/Src/app_x-cube-ai.c:50:1: warning: return type defaults to 'int' [-Wimplicit-int]
50 | LL_ATON_DECLARE_NAMED_NN_INSTANCE_AND_INTERFACE()
| ^~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~
C:/Users/tuoma/STM32Cube/helium_test/CORTEX_HELIUM/Appli/Src/app_x-cube-ai.c: In function 'LL_ATON_DECLARE_NAMED_NN_INSTANCE_AND_INTERFACE':
C:/Users/tuoma/STM32Cube/helium_test/CORTEX_HELIUM/Appli/Src/app_x-cube-ai.c:55:1: error: expected '=', ',', ';', 'asm' or '__attribute__' before '{' token
55 | {
| ^
The issue is that LL_ATON_DECLARE_NAMED_NN_INSTANCE_AND_INTERFACE is not found, but after adding
Here is the X-CUBE-AI Application config:

The model is from here https://github.com/STMicroelectronics/stm32ai-modelzoo/blob/main/audio_event_detection/yamnet/README.md
Thanks!