Skip to main content
Associate II
September 5, 2024
Solved

CubeMX not generating PLL2 code for USB

  • September 5, 2024
  • 2 replies
  • 1950 views

Hi,

I am using STM32F105RC. CubeMX does not seem to configure PLL2 at all in SystemClock_Config(). Below in the clock configurator it is clear that I have enabled PLL2 to be used for PLLCLK and USB clock.

Seems like a CubeMX bug. Or if someone can point me to what I am doing wrong that would be appreciated.

 

void SystemClock_Config(void)
{
 RCC_OscInitTypeDef RCC_OscInitStruct = {0};
 RCC_ClkInitTypeDef RCC_ClkInitStruct = {0};
 RCC_PeriphCLKInitTypeDef PeriphClkInit = {0};

 /** Initializes the RCC Oscillators according to the specified parameters
 * in the RCC_OscInitTypeDef structure.
 */
 RCC_OscInitStruct.OscillatorType = RCC_OSCILLATORTYPE_HSE;
 RCC_OscInitStruct.HSEState = RCC_HSE_ON;
 RCC_OscInitStruct.HSEPredivValue = RCC_HSE_PREDIV_DIV5;
 RCC_OscInitStruct.HSIState = RCC_HSI_ON;
 RCC_OscInitStruct.Prediv1Source = RCC_PREDIV1_SOURCE_PLL2;
 RCC_OscInitStruct.PLL.PLLState = RCC_PLL_ON;
 RCC_OscInitStruct.PLL.PLLSource = RCC_PLLSOURCE_HSE;
 RCC_OscInitStruct.PLL.PLLMUL = RCC_PLL_MUL6;
 RCC_OscInitStruct.PLL2.PLL2State = RCC_PLL_NONE;
 if (HAL_RCC_OscConfig(&RCC_OscInitStruct) != HAL_OK)
 {
 Error_Handler();
 }

 /** Initializes the CPU, AHB and APB buses clocks
 */
 RCC_ClkInitStruct.ClockType = RCC_CLOCKTYPE_HCLK|RCC_CLOCKTYPE_SYSCLK
 |RCC_CLOCKTYPE_PCLK1|RCC_CLOCKTYPE_PCLK2;
 RCC_ClkInitStruct.SYSCLKSource = RCC_SYSCLKSOURCE_HSE;
 RCC_ClkInitStruct.AHBCLKDivider = RCC_SYSCLK_DIV1;
 RCC_ClkInitStruct.APB1CLKDivider = RCC_HCLK_DIV1;
 RCC_ClkInitStruct.APB2CLKDivider = RCC_HCLK_DIV1;

 if (HAL_RCC_ClockConfig(&RCC_ClkInitStruct, FLASH_LATENCY_1) != HAL_OK)
 {
 Error_Handler();
 }
 PeriphClkInit.PeriphClockSelection = RCC_PERIPHCLK_USB;
 PeriphClkInit.UsbClockSelection = RCC_USBCLKSOURCE_PLL_DIV2;
 if (HAL_RCCEx_PeriphCLKConfig(&PeriphClkInit) != HAL_OK)
 {
 Error_Handler();
 }

 /** Configure the Systick interrupt time
 */
 __HAL_RCC_PLLI2S_ENABLE();
}


Screenshot from 2024-09-05 13-46-52.png

Best answer by mƎALLEm

Fixed in CubeMx version 6.13.0.

2 replies

mƎALLEm
Technical Moderator
September 5, 2024

But here you're setting the system clock config to HSE not to PLL. Or I didn't understand your question?

Screenshot from 2024-09-05 13-46-52.png

Associate II
September 5, 2024

Thanks for the reply!

The PLL is used for USB clock, and I have the USB OTG peripheral enabled. Is it not expected for CubeMX to generate clock configuration code for USB? Or does that clock configuration code live elsewhere?

mƎALLEm
Technical Moderator
September 5, 2024

Normally this is the USB clock config:

 PeriphClkInit.PeriphClockSelection = RCC_PERIPHCLK_USB;
 PeriphClkInit.UsbClockSelection = RCC_USBCLKSOURCE_PLL_DIV2;
 if (HAL_RCCEx_PeriphCLKConfig(&PeriphClkInit) != HAL_OK)
 {
 Error_Handler();
 }

Do you expect something else?

mƎALLEm
mƎALLEmBest answer
Technical Moderator
November 27, 2024

Fixed in CubeMx version 6.13.0.