CubeMX Route Opamp output to ADC on STM32U3C5CIUxQ
Hello,
According to Table 246 in section 27.3.3 Signal Routing of the STM32U3 Reference Manual, I should be able to configure ADC1_IN6 as an ADC input when using OPAMP1, or ADC1_IN13/ADC2_IN9 when using OPAMP2 such that the output of the opamps are routed internally to the input of the ADC.

However, in CubeMX configuration for this device, enabling the Opamp in any capacity "red's out" the option to use the corresponding ADC input for any of these combinations. In this example, OPAMP1 is set to PGA Not Connected, and I am unable to configure the ADC input on IN6.

Am I doing something wrong here, or is this simply a bug related to the recent release of this product?
Thanks!
CubeMX version: 6.17.0
OS: Ubuntu 24.04.4
Device: STM32U3C5CIUxQ