Different FreeRTOS in latest CubeMX?
Hi,
I just updated CubeIDE/CubeMX, and after creating a new project, I began configuring the microcontroller. However, when I tried to install FreeRTOS, it didn’t seem to be available. In the older version of CubeMX, there was a FreeRTOS option under Middleware (as shown in the first screenshot from a video), but it appears to be missing now. I did find X-CUBE-FREERTOS, but it doesn’t seem to offer any options like CMSIS_V1 or CMSIS_V2 or any ther very many parameters that FreeRTOS that in the previous version were available.
What happened?
1. Is that X-CUBE-FREERTOS, the only or perhaps the preferred option to use/install hrough MX?
2. How do I select CMSIS_V1 or CMSIS_V2 and all other parameters like in the older configurator (third screenshot)?
3. Are all ST libraries that rely on FreeRTOS now using X-CUBE-FREERTOS?
Thanks you :)
Ricko