Elf file - 2 or more segments define the same memory zone?
This is for a STM32H70
When uploading from CubeMx IDE or STM32CubeProgrammer I get these errors:
STM32CubeProgrammer:
Warning: File corrupted, Two or more segments defines the same memory area.
17:11:15 : Number of segments: 6
17:11:15 : segment[0]: address= 0x20000000, size= 0x0
17:11:15 : segment[1]: address= 0x20010000, size= 0x0
17:11:15 : segment[2]: address= 0x24080000, size= 0x0
17:11:15 : segment[3]: address= 0x30000000, size= 0x0
17:11:15 : segment[4]: address= 0x38000000, size= 0x0
17:11:15 : segment[5]: address= 0x90000000, size= 0x1143A8
17:11:16 : Warning: File corrupted. Two or more segments defines the same memory zone
CubeMx IDE:
"
Error in final launch sequence:
Failed to execute MI command:
load ... .elf
Error message from debugger back end:
Error finishing flash operation
Failed to execute MI command:
load ... .elf
Error message from debugger back end:
Error finishing flash operation
Failed to execute MI command:
load ... .elf
Error message from debugger back end:
Error finishing flash operation
"
The project is using external QSPI for ROM and is defined in the ld file as:
MEMORY
{
ITCMRAM (xrw) : ORIGIN = 0x00000000, LENGTH = 64K
QSPI (rx) : ORIGIN = 0x90000000, LENGTH = 8M
DTCMRAM1 (xrw) : ORIGIN = 0x20000000, LENGTH = 64K
DTCMRAM2 (xrw) : ORIGIN = 0x20010000, LENGTH = 64K
RAM (xrw) : ORIGIN = 0x24000000, LENGTH = 512K
RAM_NOCACHE (xrw) : ORIGIN = 0x24080000, LENGTH = 1024K - 512K
RAM_CD (xrw) : ORIGIN = 0x30000000, LENGTH = 128K
RAM_SRD (xrw) : ORIGIN = 0x38000000, LENGTH = 32K
}
The project compiles fine and the Build analyser reports all memory populated as expected
but when QSPI exceeds around 1MB I cannot upload to the device due to aforementioned.
.
I am also using a self penned "stldr" file for the w95q64 chip. It all works as expected (programs run without issue) until this memory limit is exceeded. I don't know where to correct the problem + any help wis much appreciated.