Skip to main content
KWoll.2
Associate
March 21, 2023
Solved

Error during migration of project (.ioc) from STM32CubeMX V6.5.0 to STM32CubeMX V6.8.0 (STM32Cube FW_F3 V1.11.4 used)

  • March 21, 2023
  • 1 reply
  • 1065 views

When I try to migrate project (.ioc) from STM32CubeMX V6.5.0 to STM32CubeMX V6.8.0 (STM32Cube FW_F3 V1.11.4 used) the following hint pops up:

0693W00000aJOxOQAW.jpgAfter selection of 'Migrate' or 'Continue' the following error pops up:

0693W00000aJOxnQAG.jpgMy question:

Is there a way to migrate STM32CubeMX-Project-File without using STM32CubeIDE?

Rowley CrossWorks for ARM is used for code development.

This topic has been closed for replies.
Best answer by KWoll.2

The question can be deleted. Problem was solved.

The warning was misinterpreted.

1 reply

KWoll.2
KWoll.2AuthorBest answer
Associate
March 21, 2023

The question can be deleted. Problem was solved.

The warning was misinterpreted.

Peter BENSCH
Technical Moderator
March 21, 2023

Well, it's always a good idea to leave the question and insert the answer, even if it was your own mistake - the next user with the same problem will surely be pleased. Thank you very much for your support!

When your question is answered, please mark this topic as answered by choosing Select as Best for the preferred answer. This will help other users find that answer faster.

Regards

/Peter