Skip to main content
Associate II
January 31, 2025
Solved

Error occurred while regenerating the project in STM32CubeMX 6.13.0 after adding a custom folder path.

  • January 31, 2025
  • 3 replies
  • 1880 views

I'm using STM323H755ZIT6 NUCLEO board, STM32CubeMX 6.13.0 and STM32CubeIDE 1.17.0.

In my scenario, I created a project in STM32CubeMX 6.13.0 and generated the project. After that, I opened this project in STM32CubeIDE 1.17.0 and added paths for external folders in Paths and Symbols. Later, I edited the .IOC file in STM32CubeMX and tried to regenerate the project, but an error popup appeared.
ERROR POPUPERROR POPUP

After this popup, I clicked the OK button, and STM32CubeMX showed 'Project Successfully Generated.' However, when I tried to build the project in STM32CubeIDE, it failed to build, and errors appeared, such as:

D:/NAVANEETHAN/CoffeeMaker/DisplayControl/Project/DisplayControl/CM7/Core/Src/main.c:116: undefined reference to `HAL_Init'

D:/NAVANEETHAN/InstalledSoftwares/STM32CubeIDE_1.17.0/STM32CubeIDE/plugins/com.st.stm32cube.ide.mcu.externaltools.gnu-tools-for-stm32.12.3.rel1.win32_1.1.0.202410251130/tools/bin/../lib/gcc/arm-none-eabi/12.3.1/../../../../arm-none-eabi/bin/ld.exe: 

A total of 40 errors were shown, all related to HAL and OS kernel functions.

I attached All errors in Errors.txt


anyone support about this issue
Thank you

Best answer by NavaneethanN

The file ..\STM32CubeIDE\.project needs to be removed. Reopening the project in STM32CubeMX and regenerating the code will resolve the mentioned issue.    

Thanks for support.

3 replies

Andrew Neil
Super User
January 31, 2025

@NavaneethanN wrote:

 an error popup appeared.
ERROR POPUPERROR POPUP


It tells you to check that log file - so did you?

A complex system that works is invariably found to have evolved from a simple system that worked.A complex system designed from scratch never works and cannot be patched up to make it work.
Associate II
February 1, 2025

@Andrew Neil 

yeah, but i couldn't find anything bro

Technical Moderator
January 31, 2025

Hello @NavaneethanN 

Could you provide your IOC file in order to further investigate the issue?

KR, Souhaib

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
Associate II
February 1, 2025

Hi @Souhaib MAZHOUD 

i attached the IOC file

NavaneethanNAuthorBest answer
Associate II
February 14, 2025

The file ..\STM32CubeIDE\.project needs to be removed. Reopening the project in STM32CubeMX and regenerating the code will resolve the mentioned issue.    

Thanks for support.