Example not showing in CubeMX Example Selector after adding to STM32Cube Pack
- December 6, 2025
- 1 reply
- 736 views
Hello,
I’ve created a custom STM32Cube Pack using STM32Cube Pack Creator and added an example project inside the pack. The pack builds successfully and installs correctly in CubeMX. However, the example I added does not appear in the CubeMX Example Selector.
It appears in "Repository/Packs" in my user folder in c:/
Details:
Pack created with STM32Cube Pack Creator
Example project added under the Examples folder in the pack structure
Pack installs fine and is visible in CubeMX
The example does not show up in the CubeMX Example Selector list
Questions:
Are there specific requirements or metadata (e.g., .pdsc file entries, example description XML) that must be included for CubeMX to recognize and display the example?
Could this be related to the folder structure or naming conventions inside the pack?
Any guidance or documentation on ensuring custom examples appear in CubeMX would be appreciated.
Thanks in advance for your help!