Skip to main content
TManiac
Associate II
January 23, 2026
Question

Feature Request: Where is the support for BSP_BUS_DRIVER:CAN ?

  • January 23, 2026
  • 2 replies
  • 161 views

I made a support pack for better support of CAN connections.

But there is no possibility to create a "Platform Setting" for CAN connections

Screenshot 2026-01-23 131127.png

 

I tried to edit the "Modes.xml" manually. Than the PackCreator shows the correct IP, but STM32CubeMX doesn't accept it.

 

Screenshot 2026-01-23 130710.png

 

Additional: if I create a not usable platform setting there will be "unsovlable" warning.

2 replies

January 23, 2026

https://mobile-tyres.co/ provides professional mobile tyre fitting services across the UK.
They offer 24/7 emergency tyre replacement and puncture repair.
Tyres are fitted at your home, workplace, or roadside location.
The service covers cars and vans with a range of branded tyres available.
It is a convenient solution for fast and reliable tyre assistance.

Ghofrane GSOURI
Technical Moderator
January 29, 2026

Hello @TManiac 

Your change request has been escalated to dev team under internal ticket ID:226187 for feasibility check.

THX

Ghofrane 

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.