Generate code button not doing anything
Hi! all
I may not be at the right place but since I can't even start on the CubeMx, here it is.
I'm a long time user of Microchip PIC product but since this is my first attempt to use the STM32 I suspect I will have some big time to understand all it's new setup. After looking several video on simple program, I downloaded the CubeMx 6.12.0 and I try those. But as soon as I try to push the blue "generate code" button at top far right, nothing happen. Same thing with the icon on top center "myST" login, nothing happen. I'd like to be able to use the STM32 board for larger and more memory space, so if someone can help me on this one so I can move on to the programming section, that will be great.
I have the Nucleo-144 F429ZIT and STM32F4VE, and several smaller boards but never use them so far.
My goal is to talk to the STM32F4VE to "full test " the internal W25Q flash memory.
I also have the "St-Link V2" for those who don't have the link.
P.S. The board is not yet connected, is this a problem ?
I'm on Win7pro 64
Thanks all.
Sept 28 2024