Generated uVision Project File is corrupted
When generating code in CubeMX for the MDK-ARM Toolchain, the uVision Project file (.uvprojx) is corrupted.
When I try to open the project it shows the following message:

Comparing the project files shows that the following section gets removed:

Manually adding this section back solves the problem temporarily until the next code generation is done.
What could be the cause for this?
I´ve already tried different versions of STM32CubeMX and uVision.
Current Versions: CubeMX: 6.14.0
uVision: 5.41
STM32U585 V 1.7.0