Question
How configure LwIP to receive UDP broadcast using STM32CubeMx ?
Hello,
I need to receive UDP Broadcast, but The "callback" function is never called.
"No broadcast" UDP communication works fine.
Is IwIP at all able to receive UDP broadcast?
I use LwIP 2.0.3, STM32F407, PHY DP83848
/*----- Default Value for IP_SOF_BROADCAST: 0 ---*/
#define IP_SOF_BROADCAST 1
/*----- Default Value for IP_SOF_BROADCAST_RECV: 0 ---*/
#define IP_SOF_BROADCAST_RECV 1
void udp_server_init(void)
{
struct udp_pcb *upcb;
err_t err;
upcb = udp_new();
ip_set_option(upcb, SOF_BROADCAST);
if (upcb)
{
err = udp_bind(upcb, IP_ADDR_BROADCAST, 8000);
if(err == ERR_OK)
{
udp_recv(upcb, udp_receive_callback, NULL);
}
}
}
void udp_receive_callback(void *arg, struct udp_pcb *upcb, struct pbuf *p, const ip_addr_t *addr, u16_t port)
{
HAL_GPIO_TogglePin(GPIOE, GPIO_PIN_2);
pbuf_free(p); // Free the p buffer
//udp_transmit(upcb, addr, udp2_tx_data, udp2_tx_len);
} Thank you
Peter