How to prevent modified auto-generated code from regenerating?
/**
* @brief IWDG Initialization Function
* @PAram None
* @retval None
*/
static void MX_IWDG_Init(void)
{
/* USER CODE BEGIN IWDG_Init 0 */
/* USER CODE END IWDG_Init 0 */
/* USER CODE BEGIN IWDG_Init 1 */
/* USER CODE END IWDG_Init 1 */
hiwdg.Instance = IWDG;
hiwdg.Init.Prescaler = IWDG_PRESCALER_4;
hiwdg.Init.Window = 4095;
hiwdg.Init.Reload = 4095;
if (HAL_IWDG_Init(&hiwdg) != HAL_OK)
{
Error_Handler();
}
/* USER CODE BEGIN IWDG_Init 2 */
/* USER CODE END IWDG_Init 2 */
}Hello, apologies if the title sounds confusing, but I wasn't sure how to accurately describe my question.
So, I have the following auto-generated code for a watchdog:
/**
* @brief IWDG Initialization Function
* @PAram None
* @retval None
*/
static void MX_IWDG_Init(void)
{
/* USER CODE BEGIN IWDG_Init 0 */
/* USER CODE END IWDG_Init 0 */
/* USER CODE BEGIN IWDG_Init 1 */
/* USER CODE END IWDG_Init 1 */
hiwdg.Instance = IWDG;
hiwdg.Init.Prescaler = IWDG_PRESCALER_4;
hiwdg.Init.Window = 4095;
hiwdg.Init.Reload = 4095;
if (HAL_IWDG_Init(&hiwdg) != HAL_OK)
{
Error_Handler();
}
/* USER CODE BEGIN IWDG_Init 2 */
/* USER CODE END IWDG_Init 2 */
}However, I want to edit line 19 as seen below:
/**
* @brief IWDG Initialization Function
* @PAram None
* @retval None
*/
static void MX_IWDG_Init(void)
{
/* USER CODE BEGIN IWDG_Init 0 */
/* USER CODE END IWDG_Init 0 */
/* USER CODE BEGIN IWDG_Init 1 */
/* USER CODE END IWDG_Init 1 */
hiwdg.Instance = IWDG;
hiwdg.Init.Prescaler = IWDG_PRESCALER_4;
hiwdg.Init.Window = 4095;
hiwdg.Init.Reload = (customTimeout * 32000) / 256 / 1000 - 1;
if (HAL_IWDG_Init(&hiwdg) != HAL_OK)
{
Error_Handler();
}
/* USER CODE BEGIN IWDG_Init 2 */
/* USER CODE END IWDG_Init 2 */
}
customTimeout is a user-defined variable, which is why I don't want it to be erased whenever code is regenerated.
I am aware of the USER CODE blocks, but I don't see anyway in which I can use them. If I put line 19 in in the first 2 USER CODE blocks, they just get overwritten if I regenerate the code as there will be another "hiwdg.Init.Reload = 4095;" in the original line 19. I can't put my modified line in the third user code block, as the the watchdog would already be initialized in line 20.
Would anyone have any idea how I can overcome this issue? Thanks!