incorrect code generated for OCTOSPI on STM32H725
STM32CubeMX generates incorrect code for the OCTOSPI interface for STM32H725.
The generated code does not populate the Req2AckTime field of the OSPIM_CfgTypeDef structure, but HAL_OSPIM_Config() validates this value and throws an assertion error.
See attached configuration in STM32CubeMX. Generated code is only:
sOspiManagerCfg.ClkPort = 1;
sOspiManagerCfg.NCSPort = 1;
sOspiManagerCfg.IOLowPort = HAL_OSPIM_IOPORT_1_LOW;
// NOTE: MISSING ASSIGNMENT TO sOspiManagerCfg.Req2AckTime
if (HAL_OSPIM_Config(&hospi1, &sOspiManagerCfg, HAL_OSPI_TIMEOUT_DEFAULT_VALUE) != HAL_OK)
{
Error_Handler();
}