ioc switching
hi I'm using nucleo-h755 144 pin board, i have configured for the project, now I'm changing the mcu from stm32h745BITx 208 pin package. is there any option in stm32cubeide to import the configuration from one mcu to another mcu in cube ide without or with opening new project. since i have configured almost 142 pins in h755 nucleo board, i don't want to do it again for the 208-pin package.
i have checked in cube ide list pinout compatible mcu option is not coming for this series, previously i have used g4 series for that it is showing.
so it possible to import the nucleo h755 pin configuration to stm32h745BITx 208- pin package in cube ide or not.
please suggest some ideas, since it will reduce the some time.
regards,
Srinath