Linux CubeMX python is not working as pre/post code generation script
What I have to do that I can directly call some python scripts as pre/post code generation step with CubeMX 6.14.1 under Linux?
Currently I can execute directly the python script on a Windows Machine, but on the Linux machine nothing happens. On Linux I can execute the scripts directly from command line without CubeMX and I can execute the scripts over a bash script which is calling the python script.
- Do I need to configure anything additional?
- Is there a possibility to select which python version is used?
- Any other hint where my problem could be?

Thanks in advance
nobody