MCU initialization fail while using HSE?
I am using NUCLEO-F767ZI board where I observe that when I use the internal clock (HSI), the mcu runs fine, but when I configure the cubeMX project to run on external 8MHz clock (HSE), the mcu fails to run. Following is the code generated by CubeMX when HSE is selected:
/** System Clock Configuration
*/void SystemClock_Config(void){RCC_OscInitTypeDef RCC_OscInitStruct;
RCC_ClkInitTypeDef RCC_ClkInitStruct; RCC_PeriphCLKInitTypeDef PeriphClkInitStruct;/**Configure the main internal regulator output voltage
*/ __HAL_RCC_PWR_CLK_ENABLE();__HAL_PWR_VOLTAGESCALING_CONFIG(PWR_REGULATOR_VOLTAGE_SCALE1);
/**Initializes the CPU, AHB and APB busses clocks
*/ RCC_OscInitStruct.OscillatorType = RCC_OSCILLATORTYPE_HSE; RCC_OscInitStruct.HSEState = RCC_HSE_ON; RCC_OscInitStruct.PLL.PLLState = RCC_PLL_ON; RCC_OscInitStruct.PLL.PLLSource = RCC_PLLSOURCE_HSE; RCC_OscInitStruct.PLL.PLLM = 4; RCC_OscInitStruct.PLL.PLLN = 96; RCC_OscInitStruct.PLL.PLLP = RCC_PLLP_DIV2; RCC_OscInitStruct.PLL.PLLQ = 11; if (HAL_RCC_OscConfig(&RCC_OscInitStruct) != HAL_OK) { _Error_Handler(__FILE__, __LINE__); }/**Activate the Over-Drive mode
*/ if (HAL_PWREx_EnableOverDrive() != HAL_OK) { _Error_Handler(__FILE__, __LINE__); }/**Initializes the CPU, AHB and APB busses clocks
*/ RCC_ClkInitStruct.ClockType = RCC_CLOCKTYPE_HCLK|RCC_CLOCKTYPE_SYSCLK |RCC_CLOCKTYPE_PCLK1|RCC_CLOCKTYPE_PCLK2; RCC_ClkInitStruct.SYSCLKSource = RCC_SYSCLKSOURCE_PLLCLK; RCC_ClkInitStruct.AHBCLKDivider = RCC_SYSCLK_DIV1; RCC_ClkInitStruct.APB1CLKDivider = RCC_HCLK_DIV2; RCC_ClkInitStruct.APB2CLKDivider = RCC_HCLK_DIV2;if (HAL_RCC_ClockConfig(&RCC_ClkInitStruct, FLASH_LATENCY_3) != HAL_OK)
{ _Error_Handler(__FILE__, __LINE__); }PeriphClkInitStruct.PeriphClockSelection = RCC_PERIPHCLK_USART1|RCC_PERIPHCLK_USART2
|RCC_PERIPHCLK_USART3|RCC_PERIPHCLK_USART6 |RCC_PERIPHCLK_UART4|RCC_PERIPHCLK_UART5 |RCC_PERIPHCLK_UART7|RCC_PERIPHCLK_UART8 |RCC_PERIPHCLK_CLK48; PeriphClkInitStruct.PLLSAI.PLLSAIN = 96; PeriphClkInitStruct.PLLSAI.PLLSAIR = 2; PeriphClkInitStruct.PLLSAI.PLLSAIQ = 2; PeriphClkInitStruct.PLLSAI.PLLSAIP = RCC_PLLSAIP_DIV4; PeriphClkInitStruct.PLLSAIDivQ = 1; PeriphClkInitStruct.PLLSAIDivR = RCC_PLLSAIDIVR_2; PeriphClkInitStruct.Usart1ClockSelection = RCC_USART1CLKSOURCE_PCLK2; PeriphClkInitStruct.Usart2ClockSelection = RCC_USART2CLKSOURCE_PCLK1; PeriphClkInitStruct.Usart3ClockSelection = RCC_USART3CLKSOURCE_PCLK1; PeriphClkInitStruct.Uart4ClockSelection = RCC_UART4CLKSOURCE_PCLK1; PeriphClkInitStruct.Uart5ClockSelection = RCC_UART5CLKSOURCE_PCLK1; PeriphClkInitStruct.Usart6ClockSelection = RCC_USART6CLKSOURCE_PCLK2; PeriphClkInitStruct.Uart7ClockSelection = RCC_UART7CLKSOURCE_PCLK1; PeriphClkInitStruct.Uart8ClockSelection = RCC_UART8CLKSOURCE_PCLK1; PeriphClkInitStruct.Clk48ClockSelection = RCC_CLK48SOURCE_PLLSAIP; if (HAL_RCCEx_PeriphCLKConfig(&PeriphClkInitStruct) != HAL_OK) { _Error_Handler(__FILE__, __LINE__); }/**Configure the Systick interrupt time
*/ HAL_SYSTICK_Config(HAL_RCC_GetHCLKFreq()/1000);/**Configure the Systick
*/ HAL_SYSTICK_CLKSourceConfig(SYSTICK_CLKSOURCE_HCLK);/* SysTick_IRQn interrupt configuration */
HAL_NVIC_SetPriority(SysTick_IRQn, 15, 0);}

Am I missing something or this is a bug? I have tried using both v4.20 and v4.23 of CubeMX tool and facing the same issue. Any resolutions?
#cubemx-project #stm32f7