Skip to main content
Associate
July 2, 2025
Solved

Missing USB CDC Middleware Files After Code Generation (STM32F103C8T6 / Nucleo-F334R8, MDK-ARM)

  • July 2, 2025
  • 1 reply
  • 2839 views

Hello everyone,

I'm new to STM32 and currently working on a USB CDC (Virtual COM Port) project using STM32CubeMX with the following setup:

  • MCUs/Boards: STM32F103C8T6 and Nucleo-F334R8

  • Toolchain / IDE: MDK-ARM (Keil µVision)

  • STM32CubeMX versions tested: 6.14.1 and 6.12.1

I configured the USB peripheral in Device Only mode and enabled the Communication Device Class (CDC) in the USB Device middleware settings. I also configured the required USB pins (PA11 as USB_DM and PA12 as USB_DP) and set the USB clock source properly to ensure 48 MHz operation.

However, after generating the project, several key USB middleware source files are missing, such as:

  • usbd_core.c

  • usbd_ctlreq.c

  • usbd_ioreq.c

  • usbd_cdc.c

  • (and sometimes also usbd_cdc_if.c)

Because of this, the code fails to compile due to missing function references.


What I’ve Tried:

  • Verified USB pins (PA11, PA12) are configured

  • Mode is set to Device_Only

  • CDC class is selected in middleware

  • USB clock is 48 MHz via PLL

  • Enabled code generation options like "Delete previously generated files"

  • Completely deleted and regenerated the project multiple times

  • Tried both STM32CubeMX 6.14.1 and 6.12.1

  • Tried both STM32F103C8T6 and Nucleo-F334R8 as targets

Despite all that, the USB CDC middleware files still fail to appear in the generated code.


Additional Note:

I have confirmed that the middleware packages are installed in CubeMX, and I also reinstalled the STM32CubeF1 firmware package just to be sure.

I’m attaching my .ioc file below for reference.


My Questions:

  • Is this a known issue or limitation with STM32CubeMX when using the MDK-ARM toolchain?

  • Is there a manual way to force CubeMX to include the USB middleware files?

  • Am I missing any additional configuration step?

Thank you in advance for your help!

 

It's my 2nd day using STM32, i don't know what to do and here's the screenshootIt's my 2nd day using STM32, i don't know what to do and here's the screenshoot

 

Best answer by Mahmoud Ben Romdhane

Hello @choirulafiq29 ,

Further to your comment, I reproduced your behavior, and I did not get the compilation errors which you had encountered.

usbd_core.c ; usbd_req.c ; usbd_ioreq.c ; usbd_cdc.c are well generated.

I want to know please the F1 Firmware version.

I will be waiting for your feedback/

MahmoudBenRomdhane_0-1751621876189.png

MahmoudBenRomdhane_1-1751621908634.png

Thanks.

Mahmoud

 

 

 

1 reply

Technical Moderator
July 2, 2025

Hello @choirulafiq29 ,

 

First let me thank you for posting and welcome to the ST Community.

Your request is under investigation, and I will get back you ASAP.

I suggest also that you provide screenshot of the compilation errors.

 

Thanks.

Mahmoud

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
Associate
July 2, 2025

Screenshot 2025-07-02 165452.png

Thanks for your responses, here's the screenshoot of my compiling message error

Technical Moderator
July 4, 2025

Hello @choirulafiq29 ,

Further to your comment, I reproduced your behavior, and I did not get the compilation errors which you had encountered.

usbd_core.c ; usbd_req.c ; usbd_ioreq.c ; usbd_cdc.c are well generated.

I want to know please the F1 Firmware version.

I will be waiting for your feedback/

MahmoudBenRomdhane_0-1751621876189.png

MahmoudBenRomdhane_1-1751621908634.png

Thanks.

Mahmoud

 

 

 

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.