MMC working on M4 core but fails to Init on M7 core. Am I missing something ?
Greetings,
I am using an STM32H747 and I have been successful in configuring my eMMC in the M4 core project (Initializing the SDMMC module, linking it to a file system, ...). I can basically do everything on the M4 and it works perfectly. However, when I try to do the same on the M7 it fails. I am literally using the exact same code and the same HAL functions with the same configuration but the HAL_MMC_Init() function returns an error all the time.
Is there something that I haven't taken into account ?
PS : For the M4 project I am using STM32CubeIDE and CubeMX and for the M7 project I use Eclipse with the Sloeber tool (for Arduino boards) since I am using an Arduino Portenta H7 board and wanted to use the arduino libraries on the M7.