Skip to main content
Associate
September 15, 2024
Solved

Newbie with newbie problems Oscillator start up ?

  • September 15, 2024
  • 8 replies
  • 3713 views

Hi People,

for the since start of year i've been setting up boards with Texas C2000 , and for the past 6 months infineon tri-core processors.  I may be changing jobs and it involves STM32 so i'm getting a head start. I have a STM32373C-EVAL , as i need TFT display and CAN. i have attempted to make a 'blinky ' project. Compiles fine but when it runs it hangs on the oscilator start up . Fresh install of STM32CubeIDE so used the config tool and let it do all the defaults.. The dev kit has solder bridges for crystal - they are open , but i've let it use the PLL.  it wont let me 

John_S_0-1726412883613.png

When running in debug it 'hangs' on stopping the code , its in the error handler from the system clock settings , if i comment out the error handler it runs . 

 

void SystemClock_Config(void)

{

RCC_OscInitTypeDef RCC_OscInitStruct = {0};

RCC_ClkInitTypeDef RCC_ClkInitStruct = {0};





/** Initializes the RCC Oscillators according to the specified parameters

* in the RCC_OscInitTypeDef structure.

*/

RCC_OscInitStruct.OscillatorType = RCC_OSCILLATORTYPE_HSI;

RCC_OscInitStruct.HSIState = RCC_HSI_ON;

RCC_OscInitStruct.HSICalibrationValue = RCC_HSICALIBRATION_DEFAULT;

RCC_OscInitStruct.PLL.PLLState = RCC_PLL_ON;

RCC_OscInitStruct.PLL.PLLSource = RCC_PLLSOURCE_HSI;

RCC_OscInitStruct.PLL.PLLMUL = RCC_PLL_MUL9;

if (HAL_RCC_OscConfig(&RCC_OscInitStruct) != HAL_OK)

{

Error_Handler(); // sometimes comment this out

}



/** Initializes the CPU, AHB and APB buses clocks

*/

RCC_ClkInitStruct.ClockType = RCC_CLOCKTYPE_HCLK|RCC_CLOCKTYPE_SYSCLK

|RCC_CLOCKTYPE_PCLK1|RCC_CLOCKTYPE_PCLK2;

RCC_ClkInitStruct.SYSCLKSource = RCC_SYSCLKSOURCE_PLLCLK;

RCC_ClkInitStruct.AHBCLKDivider = RCC_SYSCLK_DIV1;

RCC_ClkInitStruct.APB1CLKDivider = RCC_HCLK_DIV1;

RCC_ClkInitStruct.APB2CLKDivider = RCC_HCLK_DIV1;



if (HAL_RCC_ClockConfig(&RCC_ClkInitStruct, FLASH_LATENCY_1) != HAL_OK)

{

// Error_Handler(); // wont get past this one either , but still runs ok ... why ?

}

}

Has anyone else have this grief ?

Are u supposed to do something about this... Other micros i've used you just set them up and job done ?!?!

 

for now i'm leaving the check commented out so i can carry on .. Some advice would be helpful though

 

Thanks In Advance

 

Best answer by mƎALLEm

@John_S 

Again check the Crystal connection or simply replace it.

8 replies

mƎALLEm
Technical Moderator
September 15, 2024

Hello @John_S and welcome to the community,

According to your Clock config and the screenshot you shared, you are using the internal clock HSI as clock source for the system not HSE (for external crystal usage):

SofLit_0-1726419849681.png

And from your code:

RCC_OscInitStruct.OscillatorType = RCC_OSCILLATORTYPE_HSI;

RCC_OscInitStruct.HSIState = RCC_HSI_ON;

RCC_OscInitStruct.HSICalibrationValue = RCC_HSICALIBRATION_DEFAULT;

RCC_OscInitStruct.PLL.PLLState = RCC_PLL_ON;

RCC_OscInitStruct.PLL.PLLSource = RCC_PLLSOURCE_HSI;

RCC_OscInitStruct.PLL.PLLMUL = RCC_PLL_MUL9;

if (HAL_RCC_OscConfig(&RCC_OscInitStruct) != HAL_OK)

That's strange!

Could you please attach your ioc file?

 

"To give better visibility on the answered topics, please click on ""Accept as Solution"" on the reply which solved your issue or answered your question."
Rob.Riggs
Senior
September 16, 2024

I don't see anything that stands out as a problem. It has been a while since I worked with an STM32F3. Are you sure that the sysclock is actually running at 36MHz when it returns with an error?

I recommend stepping through the code in the debugger to see where it is returning with an error.

Set a breakpoint on the line that calls HAL_RCC_ClockConfig() and step into that function until an error is returned. It should provide a bit more information on what is triggering the failure.

Andrew Neil
Super User
September 16, 2024

@John_S wrote:

The dev kit has solder bridges for crystal - they are open , but i've let it use the PLL.  it wont let me 

John_S_0-1726412883613.png

 


Not quite sure what you mean here?

As shown (as @mƎALLEm said) you are using HSI - is that the case which fails?

Or are you trying to use HSE, and that's the case which fails?

To use HSE, you'll need an external crystal connected - ie, the solder bridges closed

A complex system that works is invariably found to have evolved from a simple system that worked.A complex system designed from scratch never works and cannot be patched up to make it work.
John_SAuthor
Associate
September 16, 2024

config file ..

plus 

Main.c

I was going to upload the whole project but wont accept .zip ... 

Project made fresh in STM32cubeMX then loaded in to cubeIDE ..

as a test i shut down IDE .. pulled the ST/link out so no power . Put plug back in (nothing ) , reloaded IDE up loaded with debug the file that was just working ... nothing .....  i'm a bit confused 

 

 

 

void SystemClock_Config(void)

{

RCC_OscInitTypeDef RCC_OscInitStruct = {0};

RCC_ClkInitTypeDef RCC_ClkInitStruct = {0};

RCC_PeriphCLKInitTypeDef PeriphClkInit = {0};

 

/** Initializes the RCC Oscillators according to the specified parameters

* in the RCC_OscInitTypeDef structure.

*/

RCC_OscInitStruct.OscillatorType = RCC_OSCILLATORTYPE_HSI|RCC_OSCILLATORTYPE_HSE;

RCC_OscInitStruct.HSEState = RCC_HSE_ON;

RCC_OscInitStruct.HSEPredivValue = RCC_HSE_PREDIV_DIV1;

RCC_OscInitStruct.HSIState = RCC_HSI_ON;

RCC_OscInitStruct.HSICalibrationValue = RCC_HSICALIBRATION_DEFAULT;

RCC_OscInitStruct.PLL.PLLState = RCC_PLL_ON;

RCC_OscInitStruct.PLL.PLLSource = RCC_PLLSOURCE_HSE;

RCC_OscInitStruct.PLL.PLLMUL = RCC_PLL_MUL6;

if (HAL_RCC_OscConfig(&RCC_OscInitStruct) != HAL_OK)

{

Error_Handler(); // ********** Sometimes hangs here

}

 

/** Initializes the CPU, AHB and APB buses clocks

*/

RCC_ClkInitStruct.ClockType = RCC_CLOCKTYPE_HCLK|RCC_CLOCKTYPE_SYSCLK

|RCC_CLOCKTYPE_PCLK1|RCC_CLOCKTYPE_PCLK2;

RCC_ClkInitStruct.SYSCLKSource = RCC_SYSCLKSOURCE_PLLCLK;

RCC_ClkInitStruct.AHBCLKDivider = RCC_SYSCLK_DIV1;

RCC_ClkInitStruct.APB1CLKDivider = RCC_HCLK_DIV2;

RCC_ClkInitStruct.APB2CLKDivider = RCC_HCLK_DIV1;

 

if (HAL_RCC_ClockConfig(&RCC_ClkInitStruct, FLASH_LATENCY_1) != HAL_OK)

{

Error_Handler(); // ************ Hangs here if its going to

} // if i comment out this if statement the micro wont run but

// when i uncomment after and rebuild it will now run...

// strange as hell

PeriphClkInit.PeriphClockSelection = RCC_PERIPHCLK_USB|RCC_PERIPHCLK_USART2

|RCC_PERIPHCLK_CEC|RCC_PERIPHCLK_I2C1

|RCC_PERIPHCLK_I2C2|RCC_PERIPHCLK_ADC1

|RCC_PERIPHCLK_SDADC;

PeriphClkInit.Usart2ClockSelection = RCC_USART2CLKSOURCE_PCLK1;

PeriphClkInit.I2c1ClockSelection = RCC_I2C1CLKSOURCE_HSI;

PeriphClkInit.I2c2ClockSelection = RCC_I2C2CLKSOURCE_HSI;

PeriphClkInit.USBClockSelection = RCC_USBCLKSOURCE_PLL;

PeriphClkInit.CecClockSelection = RCC_CECCLKSOURCE_HSI;

PeriphClkInit.SdadcClockSelection = RCC_SDADCSYSCLK_DIV8;

PeriphClkInit.Adc1ClockSelection = RCC_ADC1PCLK2_DIV2;

 

if (HAL_RCCEx_PeriphCLKConfig(&PeriphClkInit) != HAL_OK)

{

Error_Handler();

}

HAL_PWREx_EnableSDADC(PWR_SDADC_ANALOG1);

HAL_PWREx_EnableSDADC(PWR_SDADC_ANALOG2);

}

 

mƎALLEm
Technical Moderator
September 16, 2024

Hello,

That config is different from what you posted in the first post:

SofLit_2-1726500712157.png

The first one is using HSI and now it is using HSE. Please try to not induce us to confusions during the discussions.

Are you sure X2 crystal is mounted on its socket? Is R38 soldered?

SofLit_1-1726500552699.png

 

 

 

"To give better visibility on the answered topics, please click on ""Accept as Solution"" on the reply which solved your issue or answered your question."
John_SAuthor
Associate
September 16, 2024

sorry i've been trying different configurations to see what works... I may have got mixed up between the two. 

Yes crystal is in and r38 is in (0 ohm ) 

mƎALLEm
Technical Moderator
September 16, 2024

And if you revert o the first config: HSI (remove USB function for the moment), do you get the same behavior?

SofLit_0-1726501358157.png

SofLit_1-1726501390732.png

 

 

 

"To give better visibility on the answered topics, please click on ""Accept as Solution"" on the reply which solved your issue or answered your question."
John_SAuthor
Associate
September 16, 2024

The code runs :) 

but i've had to comment out the I2C1_init  functions ...

/* Initialize all configured peripherals */

MX_GPIO_Init();

MX_ADC1_Init();

MX_COMP2_Init();

MX_HDMI_CEC_Init();

// MX_I2C1_Init();

// MX_I2C2_SMBUS_Init();

// MX_I2S1_Init();

MX_SDADC1_Init();

MX_SDADC2_Init();

MX_SPI3_Init();

MX_TSC_Init();

MX_USART2_UART_Init();

/* USER CODE BEGIN 2 */

mƎALLEm
Technical Moderator
September 16, 2024

First, in next time please use </> button to share your code. I'm editing your post then .

Second, as with HSI is working, I'm pretty sure it's something related to the crystal. Be sure the crystal has contact in the socket. Maybe to apply a bit pressure on it with your finger.

 

"To give better visibility on the answered topics, please click on ""Accept as Solution"" on the reply which solved your issue or answered your question."
John_SAuthor
Associate
September 18, 2024

after some messing , i've took the board in to work were we have some spare crystals ... we didnt have a spare 8mhz but we did have some 16's so i've tried one of those ... low and behold after changing the setup and clock config it looks like its working.  More checking as i've only quickly hooked the crystal up to try it. i'll buy a 8meg when i get chance and this will prove the point.

To be continued but thanks all 

mƎALLEm
Technical Moderator
September 18, 2024

Hello @John_S ,


@John_S wrote:

but we did have some 16's so i've tried one of those ... low and behold after changing the setup and clock config it looks like its working. 


This feedback proves my assumption: the issue was on the crystal itself ;);)

"To give better visibility on the answered topics, please click on ""Accept as Solution"" on the reply which solved your issue or answered your question."
John_SAuthor
Associate
October 29, 2024

been a while since i've checked back in , been hacking , writing , compiling and i have problem and questions , so here goes.

I have bought a new crystal and made sure its secure in the holder - this has helped loads.

i've made a project so i can run the STM32F373VC BSP driver examples - this compile , runs in debug , and will run when made as a release , also boots straight away no grief. Happy days :)

I have now made a fresh project copying across all the board support files across so i can run the display but my code has CAN and timers running as i want to display CAN data on the LCD. 

I still have boot up / start up problems . If i compile my code as a release file and load it on via the programmer press the reset it starts , if i unplug the power - it doesnt start straight away , i have to press the reset button a few times then it runs. . . Even worse is when i load the debug file up in debug when i press resume i get nothing unless i hit the reset button a few time then the code runs i can start /stop BUT the LCD is blank ... i'm a tad confused. Looking through the files i have a "startup_stm32f373vctx.s" in my fresh code and a "startup_stm32f373xc.s" in the example code. there are bits that are different.

Can anybody shed some light ? i'm trying to figure out if i have dodgy dev kit .. but then the example code is fine ( agghhh ) 

 

mƎALLEm
Technical Moderator
October 29, 2024

Hello @John_S ,

I suggest you to open a new thread for this.

Thank you.

"To give better visibility on the answered topics, please click on ""Accept as Solution"" on the reply which solved your issue or answered your question."