Nucleo-f767zi and x-nucleo-GFX02zi CubeMX and HelloWorld and unsolved dependencies
Hello,
I am new at the STM32 World.
I started to buy a nucleo-f767zi and it worked fine.
I was not able to get the debug Console running. Like other too.
Because of that I bought the extension Board x-nucleo-GFX02zi which should be working fine with the F767ZI.
Now I tried with CubeMX to installed the Hello World Example provided.
But now I get the Message that these Packets is not Support with CubeMX 6.11. It should be support by Version 6.7 until 6.8.2.
I tested 6.8.2 and 6.8 but without any changes. It seams like the SPI does not fit together. Always I got no solution found.
Does the GFX02zi can be used with the F767ZI? Or do I have to everything new.

It is possible to fix this dependencies?
These are related to Q-SPI and Memory Access.
Thanks for any help
best regards
Carsten