Nucleo STM32WL33 CMake
Board: NUCLEO-WL33 Toolchain: CMake + arm-none-eabi-gcc CubeMX version: 6.17.0 STM32CubeIDE version: 2.1.1
I am trying to run a basic STM32WL33 project generated by STM32CubeMX using the CMake toolchain instead of the native STM32CubeIDE project format.
The same CubeMX configuration, when generated as a native STM32CubeIDE project, works correctly and reaches HAL_Init() in main.c without any issue.
However, when using the CMake-based output, the firmware crashes during startup and
never reaches main().
Symptoms
- Debugger halts inside SystemInit() at line 200 (system_stm32wl3x.c), or jumps to an address outside valid memory (0x100004ee — inside the ROM region 0x10000000–0x100017FF)
Is there a known-good CMake startup/linker reference for the STM32WL33?