OCTOSPI prescaler value use in HAL seems odd
Hello everyone,
I have a question regarding the configuration of the OCTOSPI, especially the prescaler value.
I am using the UI to configure the XSPI's prescaler and setting it to 3.

The generated code is as follows. You can see that the prescaler value is set to 3.
XSPI_HandleTypeDef hospi1;
/* OCTOSPI1 init function */
void MX_OCTOSPI1_Init(void)
{
/* USER CODE BEGIN OCTOSPI1_Init 0 */
/* USER CODE END OCTOSPI1_Init 0 */
/* USER CODE BEGIN OCTOSPI1_Init 1 */
/* USER CODE END OCTOSPI1_Init 1 */
hospi1.Instance = OCTOSPI1;
hospi1.Init.FifoThresholdByte = 1;
hospi1.Init.MemoryMode = HAL_XSPI_SINGLE_MEM;
hospi1.Init.MemoryType = HAL_XSPI_MEMTYPE_MACRONIX;
hospi1.Init.MemorySize = HAL_XSPI_SIZE_128MB;
hospi1.Init.ChipSelectHighTimeCycle = 1;
hospi1.Init.FreeRunningClock = HAL_XSPI_FREERUNCLK_DISABLE;
hospi1.Init.ClockMode = HAL_XSPI_CLOCK_MODE_0;
hospi1.Init.WrapSize = HAL_XSPI_WRAP_NOT_SUPPORTED;
hospi1.Init.ClockPrescaler = 3; /*HERE value set at 3*/
hospi1.Init.SampleShifting = HAL_XSPI_SAMPLE_SHIFT_NONE;
hospi1.Init.DelayHoldQuarterCycle = HAL_XSPI_DHQC_DISABLE;
hospi1.Init.ChipSelectBoundary = HAL_XSPI_BONDARYOF_NONE;
hospi1.Init.DelayBlockBypass = HAL_XSPI_DELAY_BLOCK_BYPASS;
hospi1.Init.Refresh = 0;
if (HAL_XSPI_Init(&hospi1) != HAL_OK)
{
Error_Handler();
}
/* USER CODE BEGIN OCTOSPI1_Init 2 */
/* USER CODE END OCTOSPI1_Init 2 */
}In the function "HAL_XSPI_Init" you have this part:
/* Configure clock prescaler */
MODIFY_REG(hxspi->Instance->DCR2, XSPI_DCR2_PRESCALER,
((hxspi->Init.ClockPrescaler) << XSPI_DCR2_PRESCALER_Pos));The register is directly set with the value of "ClockPrescaler".
However, in the user manual it's written:

Meaning, that if the value "ClockPrescaler" is "3" the prescaler is actually 4.
Shouldn't the register be set with the value "ClockPrescaler - 1" instead of "ClockPrescaler" ?
____
- STM32H533RE
- STM32CubeIDE1.18.0
- STM32Cube_FW_H5_V1.5.0
- User Manual RM0481 Rev 3