Pin conditions during ST bootloader selection
Hello everybody,
for first time flash programming of private CAN bootloader i want to use the ST bootloader.
Despite of the nBoot_SEL Bit i can flash data if the flash is empty.
The bootloader mechanism is shown in Figure 55 in the AN2606.
Now the questions :
1. Do i have to set valid level for e.g the RXD pins of UART 1 and 2 and 3 or are the internal pullup R used ?
2 During scan of all possible interfaces, see Fig. 55 in AN2606, are the corresponding output pins (e.g. TXD pins) of the interfaces in Tri-state ?
E.g. UART3 is used for flash update, is it possible to use TXD of UART2 for input, that means an external driver circuit
drives into TXD of UART2 ?
3. If i use FDCAN, do i have to use FDCAN1 (PD0 and PD1, AN2606, Table95) or FDCAN2 (Manual, 2.5, page68, pins ?) ?
Thanks in advance,
BR, Kai