Problem with CubeMX after upgrading - can't open ioc file
I upgraded STM32CubeIDE to 1.14.0 and then when I went to open an ioc file I got this message:
This project was setup with STM32CubeMX V6.9.2 using STMCube FW_G0 V1.6.1.
There are two options to proceed:
-Migrate:Migrate your project using the current STM32CubeMX version (6.10.0)
-Continue: Continue to stay compatible with the old STM32CubeMX version 6.9.2
I chose the 'Migrate' option, which was probably a mistake. Now when I try to open the ioc file it just goes blank. Any advice please?
ADDED LATER: In the meantime, I tried opening a different project, but selected the 'Continue' option. Again I got a blank tab when I tried to open the .ioc file