Problems with TouchGFX 4.21.3, STM32CubeIDE 1.12.0 and STM32CubeMX 6.8.0 for STM32F769 Disco
- March 21, 2023
- 6 replies
- 4901 views
Hi,
last Friday I updated to TouchGFX 4.21.3, STM32CubeIDE 1.12.0 and STM32CubeMX 6.8.0. At the first compilation I had an error telling that cmsis_os2.h was missing. For I couldn’t fix the problem instantly I totally deinstalled these 3 programs and reinstalled them. For testing I coded a simple demo in TouchGFX and imported it into CubeIDE without any problems. When opening CubeMX I got following messages (image 4a + 4b). This project was definitely set up with TouchGFX 4.21.3 and should be encluding STMCubeMX V6.8.0. There should not be a message to ‘continue’ or ‘migrate’. A message that TouchGFX 4.21.3 is unknown is not o.k..
Further more it is impossible to install CMSIS-Pack by the 'embedded software manager'. Those packages are missing - at least for STM32F7 (image 5a + 5b).
How can I install these packages by hand or when you will have fixed this problem? I’m working with Windows 10 and with STM32F769 Disco.
Thanks for your reply
Thilo