Skip to main content
Associate
December 14, 2023
Question

Re: Connecting SD CARD to STM32H743 without level translator

  • December 14, 2023
  • 1 reply
  • 921 views

Guys I just don't get this part in CubeMX. What does it mean by "voltage converter"? Does it refer to voltage translator? In that case why would a software stack cares about a voltage translator (which is basically a 1:1 interface) and changes the signals on pin completely by selecting different modes.

 

0.png

 

 

This topic has been closed for replies.

1 reply

Technical Moderator
December 18, 2023

Hello @Mosi and welcome to the community!

 

The voltage converter refers to the voltage level conversion that takes place when interfacing with an SD card. It ensures that the signals sent by the host are compatible with the voltage requirement of the SD card.

I suggest you have a look at this Thread, it would be helpful.

 

Thank you.

Souhaib

 

 

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.