Skip to main content
Associate
November 10, 2025
Solved

SD card MBR sector readback discrepency when compared to using a PC

  • November 10, 2025
  • 1 reply
  • 197 views

Hi there! Not entirely sure if I'm missing anything here: I've been running issue when usign FatFs library with SDMMC1 on a STM32H755ZI due to the MBR sector readback been partially incorrect. Specifically during check_fs() where we check location where the ASCII for "FAT32" is store in the MBR sector (first 512bytes). The card can be verified to function correctly using HxD tool on Windows:

xh97_0-1762813771175.png

However, through SDIO on the STM32 platform, I was getting different result for the byte [82:86], as the location is completely cleared. byte[32:24] seems to be offset to a completely different location instead:

xh97_1-1762813881602.png

Here is the code snippet where I used HAL library to grab the first (block) 512bytes:

 const uint32_t BlockAdd = 0;
 const uint32_t NumberOfBlocks = 1;

 HAL_StatusTypeDef status = HAL_SD_ReadBlocks(
 hsd,
 (uint8_t*)pData, 
 BlockAdd, 
 NumberOfBlocks, 
 Timeout 
 );

 if (status == HAL_OK)
 {
 if (HAL_SD_GetCardState(hsd) != HAL_SD_CARD_TRANSFER)
 {
 return HAL_ERROR;
 }
 }

If anyone have any pointers as to why I'm seeing this behavior that would be amazing. Curiously the 0xAA55 endmark can be read back correctly.

I'm using an 8GB Sandisk HS microsd card for testing, same behavior can be observed with a 64GB UHS Samsung microsd card as well.

Best answer by Tesla DeLorean

The latter is an MBR, the Partition Table, this will typically live at Block 0, the former is the BPB for a FAT Volume

1 reply

Tesla DeLorean
Tesla DeLoreanBest answer
Guru
November 10, 2025

The latter is an MBR, the Partition Table, this will typically live at Block 0, the former is the BPB for a FAT Volume

Tips, Buy me a coffee, or three.. PayPal VenmoUp vote any posts that you find helpful, it shows what's working..
xh97Author
Associate
November 11, 2025

Aha thanks! I have definitely overlooked the fact that the BPB resides within the first block of the partition, not the entire SD card.

In order to get the BPB block shown in the former, I will need to figure out the address to which through the partition table address stored in block 0 of the SD card.