SDMMC init error since STM32CubeIDE 1.11.0 update
There is a newly introduced bug in the freshly upgraded package coming with the IDE 1.11. MX_SDMMC1_SD_Init(void) does not configure hsd1.Init.BusWide = SDMMC_BUS_WIDE_1B but directly to the final state choosen in CubeMX (in my case 4B). But the SD requires to be started and configured with 1B before switching to the final configuration. Forcing manually to 1B makes the job, but CubeMX changes it back to 4B after each generation. The easy workaround is to force 1B in the user code at the end of SD_init function.
Could you confirm this is a bug and roll back to the correct version ?