SMBus-two-wire-Interface unavailable for STM32G474RCT3
Howdy!
I'm encountering a peculiar issue using STM32CubeMX ( version 16.6.1 ) and configuring the I2C1 peripheral with firmware version STM32Cube FW_G4 V1.6.1.
In short, I'm trying to configure it for SMBus-two-wire-Interface, but this option fails to appear in the drop-down, only making SMBus-Alert-Mode available. This is a problem since the alert pin is already being utilized for a different purpose.

This appears to be true for all the I2Cx on this device, and in desperation, I checked a handful of other STMG4x microcontrollers, and this issue remains present throughout. Additionally, I randomly checked STM32H7x, and it appears these did NOT share this issue, with the SMBus-two-wire-Interface option appearing as expected.
We have a client with a tight deadline, and using SMBUS is essential. Any updates on when this could be fixed, or workarounds would be greatly appreciated.
Thanks a million in advance!