SMT32PackCreator stuck while creating pack from existing one
Hi,
as in the object I'm trying to create a new pack starting form an existing on a DFP (Device Family Package) for SMT32L4 already published, specifically this one:
Keil.STM32L4xx_DFP.2.6.2
downloadable here:
https://www.keil.arm.com/packs/stm32l4xx_dfp-keil/
We have already a custom PCB built on stm32l451rctx so my goal was to try create a custom package starting from an existing one and this is what I did:
1. Start STM32CubeMX
2. In tab "External Tools" start "STM32PackCreator"
3. Click on "Create New Project from pack"

4. Select the above mentioned pack and filled all mandatory field an start the project creation

At this point the tool is correctly able to unzip the original pack but then it got stuck there:

Checking filesystem the original pack has effectively been unzipped but don't unterstand why it got stuck:

Any help would be appreciated.
Regards,
Silvio Taurisano