Skip to main content
peterdonchev
Senior
January 16, 2025
Question

ST32CubeMX 6.13.0 STM32H747 USB_DEVICE_M4 USB_OTG_FS files not included in the generated .cmake

  • January 16, 2025
  • 2 replies
  • 819 views

STM32CubeMX 6.13.0
MCU: STM32H747
Peripheral: USB_OTG_FS
USB Class: CDC
Core: M4
FW: 1.12.1
CMake generator selected

The generated file "mx-generated.cmake" in the CM4 folder only includes the USB Class source file, but not the USB Core source files.:

 

 ../Drivers/STM32H7xx_HAL_Driver/Src/stm32h7xx_hal_pcd.c
 ../Drivers/STM32H7xx_HAL_Driver/Src/stm32h7xx_hal_pcd_ex.c
 ../Drivers/STM32H7xx_HAL_Driver/Src/stm32h7xx_ll_usb.c
 ../Common/Src/system_stm32h7xx_dualcore_boot_cm4_cm7.c
 ../Middlewares/ST/STM32_USB_Device_Library/Class/CDC/Src/usbd_cdc.c
 ./Core/Src/sysmem.c
 ./Core/Src/syscalls.c
 ./Core/Startup/startup_stm32h747xx_CM4.s

 


IOC file is attached.

2 replies

Ghofrane GSOURI
Technical Moderator
January 17, 2025

Hello @peterdonchev 

First let me thank you for posting.

I am currently verifying this internally and will keep you updated as soon as possible.

THX

Ghofrane

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
peterdonchev
Senior
January 17, 2025

Hi,
The following files must be included by the cmake generator in the mx-generated.cmake, but they are not:

    ../Middlewares/ST/STM32_USB_Device_Library/Core/Src/usbd_core.c
    ../Middlewares/ST/STM32_USB_Device_Library/Core/Src/usbd_ctlreq.c
    ../Middlewares/ST/STM32_USB_Device_Library/Core/Src/usbd_ioreq.c

Regards,
Peter
p.s.: the same happens for the M7 core.
 
Ghofrane GSOURI
Technical Moderator
January 17, 2025

Hello @peterdonchev 

Your contribution is much appreciated.

A ticket  has been escalated to the development team in order to fix this issue . Internal ticket number 200674 

I'll keep you informed about any updates.

THX

Ghofrane

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
Semer CHERNI
ST Employee
May 20, 2025

Hello @peterdonchev 

The issue is fixed in the latest release of the STM32CubeMX (6.14.0).

KR,
Semer.