STM32-G071 ADC measurements
Hello
I am currently working with the STM32G071 microcontroller and encountering an issue with the ADC when using a specific configuration.
Here is a summary of my setup:
ADC configured in "Sequencer fully configurable" mode
Scan conversion mode: Disabled
Discontinuous conversion mode: Enabled
Oversampling: Enabled (Ratio = 8x, Right bit shift = 3)
When I measure two or more channels in this setup, the last channel in the sequence shows an incorrect result, with an error of about 30%. The earlier channels in the sequence seem to be accurate.
I would like to understand if this behavior is expected due to the chosen configuration, or if there is a workaround or recommendation to avoid this issue. Any guidance or clarification would be greatly appreciated.
Thank you in advance for your support.
Best regards,