STM32CubeIDE 1.7, MCU package L4 Series 1.17 : VTOR is not initialized
In file generated by CubeMx when creating a new project, the SystemInit function does not set the register of the interrupt vector table (SCB-> VTOR) !!!
The default value is zero, which causes a crash on the first interrupt trigger, i.e. the code loops to an address 0x1FFFxxxx (system memory)
- freshly generated code
/**
* @brief Setup the microcontroller system.
* @retval None
*/
void SystemInit(void)
{
#if defined(USER_VECT_TAB_ADDRESS)
/* Configure the Vector Table location -------------------------------------*/
SCB->VTOR = VECT_TAB_BASE_ADDRESS | VECT_TAB_OFFSET;
#endif
/* FPU settings ------------------------------------------------------------*/
#if (__FPU_PRESENT == 1) && (__FPU_USED == 1)
SCB->CPACR |= ((3UL << 20U)|(3UL << 22U)); /* set CP10 and CP11 Full Access */
#endif
/* Reset the RCC clock configuration to the default reset state ------------*/
...
code of the previous version of the package
/**
* @brief Setup the microcontroller system.
* @param None
* @retval None
*/
void SystemInit(void)
{
/* FPU settings ------------------------------------------------------------*/
#if (__FPU_PRESENT == 1) && (__FPU_USED == 1)
SCB->CPACR |= ((3UL << 10*2)|(3UL << 11*2)); /* set CP10 and CP11 Full Access */
#endif
/* Reset the RCC clock configuration to the default reset state ------------*/
/* Set MSION bit */
RCC->CR |= RCC_CR_MSION;
/* Reset CFGR register */
RCC->CFGR = 0x00000000U;
/* Reset HSEON, CSSON , HSION, and PLLON bits */
RCC->CR &= 0xEAF6FFFFU;
/* Reset PLLCFGR register */
RCC->PLLCFGR = 0x00001000U;
/* Reset HSEBYP bit */
RCC->CR &= 0xFFFBFFFFU;
/* Disable all interrupts */
RCC->CIER = 0x00000000U;
/* Configure the Vector Table location add offset address ------------------*/
#ifdef VECT_TAB_SRAM
SCB->VTOR = SRAM_BASE | VECT_TAB_OFFSET; /* Vector Table Relocation in Internal SRAM */
#else
SCB->VTOR = FLASH_BASE | VECT_TAB_OFFSET; /* Vector Table Relocation in Internal FLASH */
#endif
}
why this register is no longer set with the default flash memory address ?
Thanks for your help