STM32CubeIDE appears to be missing DMA TIM15_TRIG connection option for STM32G431KB
I want to add a TIM15_TRIG connection (is this the same as TRGO?) to a DMA transfer request.
When trying to do this via STM32CubeIDE "Version: 1.11.2 Build: 14494_20230119_0724 (UTC)" I get the following options:
i.e. no option to select TIM15_TRIG, which appears to be shown to be supported in RM0440:
Could this please be added to the interface so I can set it please?
And if it cannot be set in the STM32G431KB MCU, could you please update the documentation to reflect this fact please?
Thank you.