Skip to main content
Semer CHERNI
ST Employee
July 1, 2024
Question

STM32CubeMX 6.12.0 released

  • July 1, 2024
  • 8 replies
  • 7777 views

We are pleased to announce you that the official release of STM32CubeMX V6.12.0 is available.

  • What is new in STM32CubeMX V6.12.0?
    • New MCUs/MPUs series : STM32WB0 ,STM32MP25XX and STM32C071XX
    • Add support new CPNs STM32G4: Add support STM32G4 'Z’ and STM32G414
    • New Boards are supported: NUCLEO-C071RB , NUCLEO-WB09KE ,NUCLEO-WB07CC ,NUCLEO-WB05KZ ,STM32MP257F-DK , STM32MP257F-EV1
    • Remove STM32MP15 obsolete boards from CubeMX board selector  (  STM32MP157A-DK1 , STM32MP157A-EV1, STM32MP157C-DK2,   STM32MP157C-EV1)
    • New Boards are supported by the Start from Board feature: Nucleo-WB09xx Nucleo-WB07xx ,Nucleo-WB05xx ,Nucleo-C0 , NUCLEO-G431RB ,NUCLEO-G474RE ,NUCLEO-G491RE ,NUCLEO-H503RB ,NUCLEO-U545RE ,NUCLEO-WB15CC ,NUCLEO-WB55RG ,P-NUCLEO-WB55 ,P-NUCLEO-WB55 ,NUCLEO-WL55JC1 ,NUCLEO-WL55JC2 ,NUCLEO-WBA52CG ,NUCLEO-WBA55CG
    • Add CMake support for multicontext projects (Multi-Context ,Trust zone , Multi-core)
    • Add the support of the memory management tool for STM32WB0X and H7SC microcontrollers
    • Updated STM32CubeMX management of option bytes: STM32CubeMX preserves option bytes when regenerating a project  (H7RS ,H5, U0, WBA)
    • Add support feature (Resource Isolation Framework )RIF  / RIF Aware Ips for STM32MP25
    • LPBAM : Add missing ADF1 configuration in the LPBAM function Toolbox 
    • Add support Makefile support for WB09/07/05 and H7RS
  • Main fixed issues:
    • 164664: An issue with GUI display in STM32CubeMX.
    • 166529: TRACESWO is linked to only to Arm® Cortex®-M7 for the dual-core microcontrollers in the STM32H7 series excluding the STM32H7Rx/7Sx microcontrollers.
    • 177884: Unable to uncheck the option "save power of non-active UCPD - deactive Dead Battery pull-up" for the STM32G0 series.
    • 178050: MMC interface mode is greyed out when SDMMC1 is set to"MMC 4 bit wide bus" for the STM32H5 series.
    • 178907/179287: Incomplete generated code related to the MX_ADC3_Init() function for the STM32H7 series
    • 179275: Missing init generated code related to the MX_ADC4_Init() function for the STM32U5 series
    • 179295: Wrong generated code related to the MX_ADC1_Init() function for the STM32L4 series
    • 180281: Issue with Missing 'handle_GPDMA1' in Standard Request Mode for GPDMA Configuration for the STM32U5 series
    • 180548/181495: Oversampling ratio error for ADC3 in STM32CubeMX generated code for the SSTM32H7 series but the STM32H7Rx/7Sx microcontrollers
    • 180967: Build errors in ThreadX project with exclusive selection of LL drivers for the STM32 MCUs
    • 181386: Issue with DAC to ADC internal connection in STM32CubeMX for all the STM32H7 series but the STM32H7Rx/7Sx microcontrollers.
    • 181812: Compilation error related to the custom_stm.c file for the STM32WB series
  • Known issues fixed and problems and limitations:
    • Please refer to the wiki under this link and the release note RN0094.

8 replies

Visitor II
July 1, 2024

Why does it still show that the latest version is 6.11 here???

charleshsuz_0-1719862445800.png

 

BarryWhit
Lead
July 1, 2024

> Please refer to the wiki under this link and the release note RN0094.

the link is broken. now fixed.

 

Add support new CPNs STM32G4: Add support STM32G4 'Z’ and STM32G414

  • Community Psychiatric Nurse
  • Communist Party of Nepal  
  • Common Peroneal Nerve
  • Coloured Petri Nets
  • Certified Pediatric Nurse
  • Chronic Pyelonephritis
  • Customer Priority Notice
  • Causal Probabilistic Network
  • Cognitive Packet Network
  • Custom Part Number
  • Customer Part Number
  • Catalog Part Number

Which one is it???

Ghofrane GSOURI
Technical Moderator
July 2, 2024

Hello @BarryWhit 

First let me thank you for posting.

Support new CPNs (Commercial Part Number )STM32G4
STM32G473xx
STM32G414xx

GhofraneGSOURI_0-1719910936067.png

Thx

Ghofrane

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
padawan
Senior
July 2, 2024

Sorry wrong forum...

Padawan

 

And again

Jumping around the files after Debug.

https://community.st.com/t5/stm32cubeide-mcus/jumping-to-random-file-after-pressing-run-button/m-p/691078

Again: Opening a ticket and promising to resolve it "asap" is not a solution! 

What a poor performance after several years.

Padawan

BarryWhit
Lead
July 2, 2024

Oh, so none of them were right? hillarious. Thank you.

Associate
July 5, 2024

Hi,

µC: STM32G070RBTx

after updating to 6.12.0, the code generator shows an error with the ADC configuration.

EdwinID_0-1720168918594.png

If I reset the configuration and start over, as soon as I set the Sequencer to "Not Fully Configurable", the error occurs:

EdwinID_1-1720168986170.png

Regards,

 

Edwin

Ghofrane GSOURI
Technical Moderator
July 5, 2024

Hello @EdwinID 

First let me thank you for reporting.

This issue has been raised to our dev team (internal ticket 185851).

THX

Ghofrane

 

 

 

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
AMend.7
Associate III
July 5, 2024

Hi,

What does the "OEM Restricted" Marketing Status of the new STM32G414x mean?

Ari

 

frackers
Senior
August 9, 2024

6.12 crashes when opening an existing 6.11.1 project on Linux Debian Jessie (8). Works OK on Ubuntu Jammy Jellyfish (22.04). 

Exception in thread "AWT-EventQueue-0" java.lang.NullPointerException: Cannot invoke "com.teamdev.jxbrowser.browser.Browser.mainFrame()" because "this.browser" is null

Full backtrace attached

 

Updating the project file using 6.12 on the Ubuntu system and now the project reads OK.

BTW: Good to see that the syscall & sysmem generation bugs have been fixed

ALSO: Trying to attach a file called 'bug' results in an error of 'filetype .bug not supported' . You do realise I hope that not all files have a filename extension and if it does it may not be 3 characters!!

 

 

 

Visitor II
September 4, 2024

Hi frackers, I also met same problem in Ubuntu24, did you solve your problem?